Low value is greater than high value
The low signal or low clamp limit value is greater than the high signal or high clamp limit value. The high value must be greater than the low value. Enter valid values and save the changes.
Provide Feedback