Points view parameters (output devices)
The
Points
view includes these parameters:Parameter | Description |
|---|---|
Points | Displays the point group to which this configuration applies. |
Output State During Program Mode/Fault Mode | Specifies the output state in Program or Fault mode. The valid values are:
Tip : These parameters appear shaded in Run mode. |
Latch Faults | Select the checkbox to latch alarms. The default is unlatched (cleared). Tip : The checkbox appears shaded in Run mode. |
Point Fault Reset | Select to reset latched alarms. Tip : Reset appears shaded when offline. |
Provide Feedback