Points view parameters (input devices)
The
Points
view includes these parameters:
TIP:
These parameters appear shaded in Run mode.
Parameter | Description |
|---|---|
Points | Displays the point number to which this configuration applies. |
Input Filter Time | Sets a time by which to delay the transition from Off to On or from On to Off. This feature is useful for filtering out transients in noisy environments. Select a value in milliseconds (ms). The valid range is from 0.000 through 65.535. The default value is 1.000. |
Provide Feedback