Point Operation Discrepancy Time over range
The
Point Operation Discrepancy Time
value is greater than the maximum allowed. Select a value from 10 through 65530 in increments of 10, and then apply the changes.Provide Feedback