Input Delay Time over range

The Input Delay Time is greater than the maximum allowed. Select a value from 0 through 126 in increments of 6, and then apply the changes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal