Error Latch Time over range
The
Input Error Latch Time
or Output Error Latch Time
is greater than the maximum allowed. Enter a value from 0 through 65530 in increments of 10, and then apply the changes.Provide Feedback