Tachometer view parameters

The parameters in this view
appears shaded under these conditions:
  • Run mode
  • Project Safety Secured mode
  • Point Mode
    =
    Not Used
  • Range
    Tachometer
Parameter
Description
Channel
Indicates the channel to which the configuration applies to.
Dual Low Detection
Specifies the dual low detection mode for each channel. Valid values include:
  • Off
    (default)
  • On
Trigger
Specifies the trigger mode for each channel. Valid values include:
  • Falling Edge
    (default)
  • Rising Edge
Off Level
Specifies the tachometer off level in volts for each channel. Valid values are from 0 V through 23 V. The default is 5 V.
On Level
Specifies the techometer on level in volts for each channel. Valid values are from 1 V through 24 V. The default is 11 V.
The
On Level
value must be greater than the
Off Level
value.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal