Safety Inputs view parameters
Parameter | Description |
|---|---|
Channel | Indicates the channel to which the configuration applies to. |
Type | Specifies the safety input mode for channels in pair. Valid values include:
Type appears shaded under these conditions:
|
Discrepancy Time | Displays the discrepancy time for each channel. Valid values are from 0 ms through 65530 ms in increments of 10 ms. When the device is in Equivalent mode, the default is 100 ms. Discrepancy Time appears shaded under these conditions:
|
Deadband | Displays the deadband value for each channel. Valid values are from 0 through 30000 (engineering units). The default is 0. Deadband appears shaded under these conditions:
|
Channel Offset | Displays the channel offset value. Valid values are from -32768 through 32767 (engineering units). The default is 0. Channel Offset appears shaded under these conditions:
|
Input Error Latch Time | Specifies the input error latch time. Valid values are from 0 ms through 65530 ms in increments of 10 ms. The default is 1000 ms. Input Error Latch Time appears shaded under these conditions:
|
Provide Feedback