Fault/Program Action view parameters
Parameter | Description |
|---|---|
Points | Indicates the point to which the configuration applies. |
Output State During Program Mode | Specifies the behavior of each output when the controller's mode changes to Program. Valid values are:
This parameter is not available in Run mode. |
Output State During Fault Mode | Specifies the behavior of each output when the connection from the controller to the output device is broken. Valid values are:
This parameter is not available in Run mode. |
Provide Feedback