Invalid alarm

The alarm configurations are in conflict. This error occurs in one of these conditions:
  • The high high limit value is lower than the high limit value.
  • The high limit value is lower than the low limit value.
  • The low limit value is lower than the low low limit values.
Modify your configuration and apply the changes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal