Input range is under range
The value is less than the minimum value allowed in the defined input range for this device. The valid range is from -1.0E+11 through 1.0E+11.
Enter a value within the input range for this device, and then apply the changes.
Provide Feedback