Points view parameters (input devices)
The
Points
view includes these parameters:Parameter | Description |
|---|---|
Point | Indicates the point number to which this configuration applies. |
Input Filter Time Off -> On | Defines how long an Off to On input transition must remain in the On state before the device considers the transition valid. |
Input Filter Time On -> Off | Defines how long an On to Off input transition must remain in the Off state before the device considers the transition valid. |
Enable Diagnostics | Enables short circuit and open wire detection on the point when selected. |
Provide Feedback