HART Device Information view

The
HART Device Information
view displays configuration information about the attached HART Field Device.
Use the
HART Device Information
view to:
  • View manufacturer and revision information.
  • View tag, message, and other descriptor information entered into the HART Field Device.
  • Check ranges and Primary Variable configuration.
  • Configure the tag, message, and descriptor for the HART Field Device.
  • View the SV, TV, and FV units.
  • Refresh the device information.
    TIP:
    The parameters are not available when offline or HART is not enabled for the channel.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal