Select the units for the PV range
Use
Select PV Units
to select PV units
for the PV Upper Range
and Lower Range
values.To select the units for the PV range
- On the tab for the device, expandChannels, and then expand an individual channel.
- SelectHART Command.
- In theHART Commandview, select theEnable HART Device PV Range Configuration (Command 35, Command 47)checkbox, and then select (...).
- InSelect PV Units, specify these parameters:
- CategoryCategory of the unit, such as power, electrical, and temperature. If there is no suitable category,Enter ID Valueis assigned.
- PV UnitsUnit of measure associated with the category. Not available whenCategoryis set toEnter ID Value.
- PV Unit IDUnit ID associated with the unit. WhenCategoryisEnter ID Value, a value between 1 and 255 is assigned. The default is 32.
- SelectOKto confirm and save the changes.
Provide Feedback