Device-defined data types

This table shows the device-defined data types for 1719 Analog I/O devices.
Catalog Number
Configuration
Input
Output
1719-CF4H Input Mode
AB:1718_19_AIn_HART:C:0
AB:1718_19_AIn:I:0
AB:1718_19_AIn_HART:I:0
N/A
1719-CF4H Output Mode
AB:1718_19_AOn_HART:C:0
AB:1718_19_AOn:I:0
AB:1718_19_AOn_HART:I:0
AB:1718_19_AOn:O:0
1719-IF4HB
AB:1718_19_AIn_HART:C:0
AB:1718_19_AIn:I:0
AB:1718_19_AIn_HART:I:0
N/A
1719-IR4B
AB:1718_19_RTDn:C:0
AB:1718_19_TIn:I:0
N/A
1719-IT4B
AB:1718_19_TCn:C:0
AB:1718_19_TIn:I:0
N/A
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal