Tech Access Register Map

The Tech Access Register map contains parameters used developers for testing the PQconnect board and filter or left for future implementation and is only usable for TCI, LLC.
Note:
All parameters with an asterisk (*) in the description will require the Tech level access codes parameter key A: 0x007D (125) and parameter key B: 0xEA6E (60014). All parameters are enabled for communication to EtherNet/IP unless explicitly stated otherwise in the Notes Column of the Table.
Table
15
: Tech Access Feedback and Setpoint Parameters Register Map
Parameter Name
(EtherNet/IP Name)
Instance ID
Description
Type
Default & Ranges
Notes
SYS_PEEK_0
(DiagVal0)
304
Diagnostic peek value 0
R
Default:0
A diagnostic Feedback variable used by Production and Engineering for Testing and Field Support.
SYS_PEEK_1
(DiagVal1)
305
Diagnostic peek value 1
R
Default:0
SYS_PEEK_2
(DiagVal2)
306
Diagnostic peek value 2
R
Default:0
SYS_PEEK_3
(DiagVal3)
307
Diagnostic peek value 3
R
Default:0
TEST_VOLTAGE
(TestVoltage)
13
Unit test voltage, (10 = 1.0 Volts)
R/W
Default:0
Range:0 to 6900
Factory Used Parameter. Used to check if Filter was configured with the correct test Voltage.
TEST_FREQUENCY
(TestFreq)
14
Unit test frequency, (Hz)
R/W
Default:0
Range:0 to 60
Factory Used Parameter. Used to check if Filter was configured with the correct test frequency.
SYS_POKE_0
(Poke0)
166
Diagnostic poke variable 0
R/W
Default:0
Range:-32768 to 32767
SYS_POKE_1
(Poke1)
167
Diagnostic poke variable 1
R/W
Default:0
Range:-32768 to 32767
SYS_POKE_2
(Poke2)
168
Diagnostic poke variable 2
R/W
Default:0
Range:-32768 to 32767
SYS_POKE_3
(Poke3)
169
Diagnostic poke variable 3
R/W
Default:0
Range:-32768 to 32767
SYS_PEEK_ADDR_0
(PeekAddr0)
170
Diagnostic peek address 0
R/W
Default:0
Range:0 to 65535
SYS_PEEK_ADDR_1 (PeekAddr1)
171
Diagnostic peek address 1
R/W
Default:0
Range:0 to 65535
SYS_PEEK_ADDR_2 (PeekAddr2)
172
Diagnostic peek address 2
R/W
Default:0
Range:0 to 65535
SYS_PEEK_ADDR_3 (PeekAddr3)
173
Diagnostic peek address 3
R/W
Default:0
Range:0 to 65535
BGM_PASSKEY_A_EIP (DiagFb1)
313
Diagnostic Feedback Parameter 1
R
Default:0
Ethernet Enabled but Mapped to Modbus Instance: BGM_PASSKEY_A
Read only Value of BGM Password - High Bytes
BGM_PASSKEY_B_EI
(DiagFb2)
314
Diagnostic Feedback Parameter 2
R
Default:0
"Ethernet Enabled but Mapped to Modbus Instance: BGM_PASSKEY_B
Read only Value of BGM Password - Low Bytes
DIAGONSTIC_FEEDBACK_3 (DiagFb3)
315
Diagnostic Feedback Parameter 3
R
Default:0
EtherNet Only: Reserved Does not exist in Database.
DIAGONSTIC_FEEDBACK_4 (DiagFb4)
316
Diagnostic Feedback Parameter 4
R
Default:0
SYS_COM_ACTIVE
(DiagFb5)
317
Diagnostic Feedback Parameter 5
R
Default:0
System Communication Status,
bit 0 = Modbus RTU active,
bit 1 = Bluetooth active,
bit 2 = EtherNet/IP active
SYS_CNT_MIN_OFF_TIMER_EIP (DiagFb6)
318
Diagnostic Feedback Parameter 6
R
Default:0
Ethernet Enabled but Mapped to Modbus Instance: SYS_CNT_MIN_OFF_TIMER
Displays count down time for contactor re-closures.
Once this timer expires contactor will change the contactor state to close.
Default: 60 seconds
Range: 30 to 300 seconds
PARAM_ACCESS_LEVEL_EIP (DiagFb7)
319
Diagnostic Feedback Parameter 7
R
Default:0
Ethernet Enabled but Mapped to Modbus Instance: PARAM_ACCESS_LEVEL_RO
Determines the Level of parameter access to read and/or change parameter inputs.
0 = Base access
1 = Tech access
2 = Factory access
DIAGONSTIC_FEEDBACK_9 (DiagFb9)
320
Diagnostic Feedback Parameter 7
R
Default:0
EtherNet Only: Reserved Does not exist in Database
DIAGONSTIC_FEEDBACK_10 (DiagFb10)
321
Diagnostic Feedback Parameter 10
R
Default:0
DIAGONSTIC_FEEDBACK_11 (DiagFb11)
322
Diagnostic Feedback Parameter 10
R
Default:0
DIAGONSTIC_FEEDBACK_12 (DiagFb12)
323
Diagnostic Feedback Parameter 12
R
Default:0
DIAGONSTIC_FEEDBACK_13 (DiagFb13)
324
Diagnostic Feedback Parameter 13
R
Default:0
DIAGONSTIC_FEEDBACK_14 (DiagFb14)
325
Diagnostic Feedback Parameter 14
R
Default:0
DIAGONSTIC_FEEDBACK_15 (DiagFb15)
326
Diagnostic Feedback Parameter 15
R
Default:0
DIAGONSTIC_FEEDBACK_16 (DiagFb16)
327
Diagnostic Feedback Parameter 16
R
Default:0
DIAGONSTIC_FEEDBACK_8 (DiagFb8)
328
Diagnostic Feedback Parameter 8
R
Default:0
DIAG_SETPOINT_1
(DiagSP1)
190
Diagnostic Setpoint Parameter 1
R/W
Default:0
Range:0 to 0
EtherNet Only: Reserved Does not exist in Database.
DIAG_SETPOINT_2
(DiagSP2)
191
Diagnostic Setpoint Parameter 2
R/W
Default:0
Range:0 to 0
DIAG_SETPOINT_3
(DiagSP3)
192
Diagnostic Setpoint Parameter 3
R/W
Default:0
Range:0 to 0
DIAG_SETPOINT_4
(DiagSP4)
193
Diagnostic Setpoint Parameter 4
R/W
Default:0
Range:0 to 0
DIAG_SETPOINT_5
(DiagSP5)
194
Diagnostic Setpoint Parameter 5
R/W
Default:0
Range:0 to 0
DIAG_SETPOINT_6
(DiagSP6)
195
Diagnostic Setpoint Parameter 6
R/W
Default:0
Range:0 to 0
DIAG_SETPOINT_7
(DiagSP7)
196
Diagnostic Setpoint Parameter 7
R/W
Default:0
Range:0 to 0
DIAG_SETPOINT_8
(PROC_DATA_CMD_EN)
197
Diagnostic Setpoint Parameter 8
R/W
Default:0
Range:0 to 1
Enables and Disables Implicit Setpoint Writes.
Only used for Passive Filters with EtherNet/IP Connectivity.
0 = Implicit IO Writes Disabled
1 = Implicit IO Writes Enabled
DIAG_SETPOINT_9
(DiagSP9)
198
Diagnostic Setpoint Parameter 9
R/W
Default:0
Range:0 to 0
EtherNet Only: Reserved Does not exist in Database.
DIAG_SETPOINT_10
(DiagSP10)
199
Diagnostic Setpoint Parameter 10
R/W
Default:0
Range:0 to 0
DIAG_SETPOINT_11
(DiagSP11)
200
Diagnostic Setpoint Parameter 11
R/W
Default:0
Range:0 to 0
DIAG_SETPOINT_12
(DiagSP12)
201
Diagnostic Setpoint Parameter 12
R/W
Default:0
Range:0 to 0
DIAG_SETPOINT_13
(DiagSP13)
202
Diagnostic Setpoint Parameter 13
R/W
Default:0
Range:0 to 0
DIAG_SETPOINT_14
(DiagSP14)
203
Diagnostic Setpoint Parameter 14
R/W
Default:0
Range:0 to 0
DIAG_SETPOINT_15
(DiagSP15)
204
Diagnostic Setpoint Parameter 15
R/W
Default:0
Range:0 to 0
DIAG_SETPOINT_16
(DiagSP16)
205
Diagnostic Setpoint Parameter 16
R/W
Default:0
Range:0 to 0
V_OUT_FUND_HZ
(FFund)
270
Load output voltage fundamental frequency, (Hz)
R
Default:0
V_IN_CARRIER_HZ
(FCarrier)
271
Estimated input voltage carrier frequency, (Hz)
R
Default:0
FUND_TRACKING_MODE (FundFreqTrackMode)
111
Fundamental frequency tracking mode
R/W
Default:0
Range:0 to 0
FUND_TRACKING_FILTER
_GAIN (FundFreqFiltGain)
112
Fundamental frequency reference filter gain
R/W
Default:0
Range:0 to 0
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal