Status Register Map
This register map contains Filter and Line Status parameters used by the passive filter. Please reference the Filter Status Table in the IOM if needed.
Note:
All parameters with an asterisk (*) in the description will require the Tech level access codes parameter key A: 0x007D (125) and parameter key B: 0xEA6E (60014). All parameters are enabled for communication to EtherNet/IP unless explicitly stated otherwise in the Notes Column of the Table.
Table
1
: Status Feedback and Setpoint Parameters Register Map
Parameter Name (EtherNet/IP Name) | Instance ID | Description | Type | Default & Ranges | Notes |
USER_STATE (UserState) | 206 | User State | R | Default:0 | User State Parameter 00 = INIT_START 01 = INIT_DELAY 02 = INIT_E2_CHIP 03 = INIT_FLASH_TEST 04 = WRITE_FLASH_TEST 05 = SETUP_FLASH 06 = SETUP_NON_CAL_FLASH 07 = SAVE_CURRENT_VALUES 08 = STAMP_EE 09 = INIT_FROM_DEFAULTS 10 = INIT_FROM_FLASH 11 = EXECUTE_PARAM_FUNCTIONS 12 = PARAM_INIT_FINISH 13 = RESTORE_DEFAULTS 14 = RESTORE_NON_CAL_DEFAULT 15 = INIT_SAVE_CURRENT_VALUES 16 = REBOOT 17 = SETUP_UNIT_CAL_FLASH 18 = RESTORE_UNIT_CAL_DEFAULT 19 = UPDATE_EEPROM 20 = UNPROTECT_EEPROM 21 = PROTECT_EEPROM |
CNT_CLOSED (CntClosed) | 272 | Filter tuned circuit contactor closed | R | Default:0 | Indicates the status of the Filters tuned circuit contactor. 0 = Contactor Closed 1 = Contactor Open |
SYS_POWER_ON (PowerOn) | 273 | Filter powered on | R | Default:0 | Indicates if the filter has input power available 0 = Power Off 1 = Power On |
SYS_STATUS_OK (StatusOK) | 274 | Filter status OK | R | Default:0 | Indicates filters status 0 = Filter is operating 1 = Filter has indicated status warning |
SYS_AT_CAPACITY (AtCapacity) | 275 | Filter at maximum capacity | R | Default:0 | Indicates if the filter is running at its maximum current capacity 0 = Nominal 1 = At Capacity |
STATUS_FILTER_A (FilterStatusActiveA) | 279 | Filter status detection active A bit mask | R | Default:0 | Reference Filter Status Table in IOM To enabled desired status detections, enter bit mask from table by converting to decimal Range: 0 to 65535 |
STATUS_FILTER_B (FilterStatusActiveB) | 280 | Filter status detection active B bit mask | R | Default:0 | |
STATUS_LINE (LineStatusActive) | 281 | Line status detection active bit mask | R | Default:0 | Reference Filter Status Table in IOM To enabled desired status detections, enter bit mask from table by converting to decimal Range: 0 to 65535 |
STATUS_FILTER_LOAD (LoadStatusActive) | 282 | Filter load status detection bit mask | R | Default:0 | Reference Filter Status Table in IOM To enabled desired status detections, enter bit mask from table by converting to decimal Range: 0 to 65535 |
STATUS_FILTER_A_ENABLE_RO (FilterStatusEnabledA) | 283 | Filter status A detection enable bit mask | R | Default:0 | Reference Filter Status Table in IOM To enabled desired status detections, enter bit mask from table by converting to decimal Range: 0 to 65535 |
STATUS_FILTER_B_ENABLE_RO (FilterStatusEnabledB) | 284 | Filter status B detection enable bit mask | R | Default:0 | |
STATUS_LINE_ENABLE_RO (LineStatusEnabled) | 285 | Line status detection enable bit mask | R | Default:0 | Reference Filter Status Table in IOM To enabled desired status detections, enter bit mask from table by converting to decimal Range: 0 to 65535 |
STATUS_FILTER_LOAD_ENABLE_RO (LoadStatusEnabled) | 286 | Filter load status detection enable bit mask | R | Default:0 | Reference Filter Status Table in IOM To enabled desired status detections, enter bit mask from table by converting to decimal Range: 0 to 65535 |
PARAM_STATE (ParamState) | 287 | Parameter state | R | Default:0 | Indicates the present state of the parameter state machine. 00 = INIT_START 01 = INIT_DELAY 02 = INIT_E2_CHIP 03 = INIT_FLASH_TEST 04 = WRITE_FLASH_TEST 05 = SETUP_FLASH 06 = SETUP_NON_CAL_FLASH 07 = SAVE_CURRENT_VALUES 08 = STAMP_EE 09 = INIT_FROM_DEFAULTS 10 = INIT_FROM_FLASH 11 = EXECUTE_PARAM_FUNCTIONS 12 = PARAM_INIT_FINISH 13 = RESTORE_DEFAULTS 14 = RESTORE_NON_CAL_DEFAULTS 15 = INIT_SAVE_CURRENT_VALUES 16 = REBOOT 17 = SETUP_UNIT_CAL_FLASH 18 = RESTORE_UNIT_CAL_DEFAULTS 19 = UPDATE_EEPROM 20 = UNPROTECT_EEPROM 21 = PROTECT_EEPROM |
SYS_STATE (SysState) | 288 | System state | R | Default:0 | Indicates the present state of the system state machine (Read Only) 00 = Initialization State Machine 01 = Initialization Parameters 02 = Power on Delay 03 = Unit State Configuration Check 04 = Reset 05 = Force Open Contactor 06 = Force Close Contactor 07 = Auto Load Open 08 = Auto Load Close 09 = Auto kVAR Close 10 = Auto kVAR Open 11 = External Open 12 = External Close 13 = No Contactor 14 = Contactor Closed Inhibited 15 = Calibrate offsets 16 = Calibrate Magnitude 17 = No Communication 18 = Communication configuration 19 = PCB Calibration Check 20 = Unit Calibration Check 21 = Pre-Calibration Check 22 = Unit in Contactor Debug Close |
CNT_STATUS (CntStatus) | 289 | Contactor command status | R | Default:0 | Indicates the present contactor status command, 00 = Init State at Startup 01 = Force Close Condition 02 = Force Open Condition 03 = Auto Load Open Condition 04 = Auto kVAR Open Condition 05 = External Open Condition 06 = No Contactor Condition 07 = Contactor Open 08 = Contactor Param Inhibit 09 = Contactor Power On Inhibit 10 = Contactor Calibrate Inhibit 11 = Contactor Min Reclose 12 = Contactor Close Delay 13 = Contactor Auto Reclose Delay 14 = Contactor Auto Reclose Limit 15 = Contactor Config Inhibit |
RELAY_INPUT_STATUS (RelayInputStatus) | 290 | Digital relay input status | R | Default:0 | Filter Relay Input Status, 0b00 = Relay 1 (Temp Okay), Relay 2 (Temp Okay) 0b01 = Relay 1 (Temp Hot), Relay 2 (Temp Okay) 0b10 = Relay 1 (Temp Okay), Relay 2 (Temp Hot) 0b11 = Relay 1 (Temp Hot), Relay 2 (Temp Hot) |
FIELDBUS_STATUS_A (FBStatusA) | 294 | Field Bus communication status A Register | R | Default:0 | Ethernet Module Status Register A Notifies the User of the status of the EtherNet/IP Module. |
FIELDBUS_STATUS_B (FBStatusB) | 295 | Field Bus communication status B Register | R | Default:0 | Ethernet Module Status Register B Notifies the User of the status of the EtherNet/IP Module. |
SYS_NULL_STAT (PCBCalStatus) | 296 | Factory PCB calibration status | R | Default:0 | System PCB Calibration Status 0 = Not Calibrated 1 = PCB Calibrated (Completed by Factory) |
SYS_MAG_CAL_STATUS (UnitCalStatus) | 300 | Unit calibration completed status | R | Default:0 | Six-bit bitmask of Calibration Status of Current Channels 0b000001 = channel 1 cal complete 0b000011 = channel 1 and 2 cal complete 0b111111 = channel 1 to 6 cal complete |
HISTORY_LOG_STATUS (HistoryLogStatus) | 312 | History Log Status Value | R | Default:0 | Indicates Status of the History Log 0 = Initializing History Log 1 = Successfully Reading History 2 = Out of Bounds history register 3 = EEPROM is busy |
STATUS_FILTER_A_RELAY_ACTION (FilterStatusRelayAEn) | 15 | Filter status A relay action enable bit mask | R/W | Default:9 Range:0 to 65535 | Reference Filter Status Table To Enable desired status detections, enter bit mask from table by converting to decimal. If a status is active and the bit corresponding to that status in this mask is set, the relay will be activated. 0 = Disabled 65535 = All enabled |
STATUS_FILTER_B_RELAY_ACTION (FilterStatusRelayBEn) | 16 | Filter status B relay action enable bit mask | R/W | Default:49151 Range:0 to 65535 | |
STATUS_LINE_RELAY_ACTION (LineStatusRelayEn) | 17 | Line status relay action enable bit mask | R/W | Default:71 Range:0 to 65535 | Reference Line Status Detection bits To Enable desired status detections, enter bit mask from table by converting to decimal. If a status is active and the bit corresponding to that status in this mask is set, the relay will be activated 0 = Disabled 65535 = All enabled |
STATUS_FILTER_LOAD_RELAY_ACTION (LoadStatusRelayEn) | 18 | Filter load status relay action enable bit mask | R/W | Default:63 Range:0 to 65535 | Reference load status detection bits table To Enable desired status detections, enter bit mask from table by converting to decimal. If a status is active and the bit corresponding to that status in this mask is set, the relay will be activated. 0 = Disabled 65535 = All enabled |
STATUS_FILTER_A_CNT_ACTION (FilterStatusCntAEn) | 19 | Filter status A tune contactor action enable bit mask | R/W | Default:1 Range:0 to 65535 | Reference Filter Status Table in IOM To enabled desired status detections, enter bit mask from table by converting to decimal.0 = Disabled 65535 = All enabled |
STATUS_FILTER_B_CNT_ACTION (FilterStatusCntBEn) | 20 | Filter status B tune contactor action enable bit mask | R/W | Default:36863 Range:0 to 65535 | |
STATUS_LINE_CNT_ACTION (LineStatusCntEn) | 21 | Line status tune contactor action enable bit mask | R/W | Default:64 Range:0 to 65535 | Reference Line Status Detection bits To Enable desired status detections, enter bit mask from table by converting to decimal. If a status is active and the bit corresponding to that status in this mask is set, the relay will be activated 0 = Disabled 65535 = All enabled |
STATUS_FILTER_LOAD_CNT_ACTION (LoadStatusCntEn) | 22 | Filter load status tune contactor action enable bit mask | R/W | Default:0 Range:0 to 65535 | Reference load Status Table in IOM To enabled desired status detections, enter bit mask from table by converting to decimal.0 = Disabled 65535 = All enabled |
HISTORY_LOG_REQUEST (HistReqCmd) | 189 | Status detection history record request command | R/W | Default:0 |
Provide Feedback