Read Only Register Map
Note that some parameters shown below may not exist in the parameter database/ or shown in PQVision. These parameters have been reserved for future use.
Note:
All parameters with an asterisk (*) in the description will require the Tech level access codes parameter key A: 0x007D (125) and parameter key B: 0xEA6E (60014). All parameters are enabled for communication to EtherNet/IP unless explicitly stated otherwise in the Notes Column of the Table.
Table
16
: Read Only Feedback and Setpoint Parameters Register Map
Parameter Name (EtherNet/IP Name) | Instance ID | Description | Type | Default & Ranges | Notes |
DSP_MODEL_NUM_RO (DSPModelNum) | 208 | Digital Signal Processor DSP model number | R | System Model Numbers 0 = Undefined 3 = Sim 101 = HSD 102 = HGL 103 = HGP 104 = HSL 105 = HSE 200 = KIT - BLANK 202 = KIT - HGL 203 = KIT - HGP 205 = KIT – HSE | |
HMS_MODEL_NUM_RO (FBModelNum) | 210 | Fieldbus communications processor model number | R | Default:0 | Ethernet Hardware Version Number Notifies the user what type of Module is connected. |
BGM_MODEL_NUM_RO (WLModelNum) | 212 | Wireless communications firmware model number | R | Default:0 | Module Revision Code for Bluetooth Processor 0 = Null 1 = BGM111 2 = BGM210 3 = BGM220 |
Provide Feedback