Onset and Delay Register Map

The Onset and Delay Register map contains parameters used by the PQconnect board for fault and status detection logic. Onset is the level at which the fault/status detection activates changing the threshold can cause fault to occur earlier or later. Clear is the level at which the fault/status detection is deemed no longer present and allowing the filter to return to normal operation. Note that some parameters shown below may not exist in the parameter database/ or shown in PQVision. These parameters have been reserved for future use.
Note:
All parameters with an asterisk (*) in the description will require the Tech level access codes parameter key A: 0x007D (125) and parameter key B: 0xEA6E (60014). All parameters are enabled for communication to EtherNet/IP unless explicitly stated otherwise in the Notes Column of the Table.
Table
14
: Onset and Delay Feedback and Setpoint Parameters Register Map
Parameter Name
(EtherNet/IP Name)
Instance ID
Description
Type
Default & Ranges
Notes
V_LINE_OV_ONSET (VLineOVOnset)
43
Overvoltage onset threshold, (percent rated voltage)
R/W
Default:130
Range:100 to 150
V_LINE_OV_CLEAR
(VLineOVClear)
44
Overvoltage clear threshold, (percent rated voltage)
R/W
Default:125
Range:90 to 140
V_LINE_OV_DELAY (VLineOVDelay)
45
Overvoltage delay time, (sec)
R/W
Default:2
Range:1 to 3600
V_LINE_UV_ONSET (VLineUVOnset)
46
Undervoltage phase loss onset threshold, (percent rated voltage)
R/W
Default:75
Range:50 to 90
V_LINE_UV_CLEAR
(VLineUVClear)
47
Undervoltage phase loss clear threshold, (percent rated voltage)
R/W
Default:80
Range:60 to 100
V_LINE_UV_DELAY
(VLineUVDelay)
48
Undervoltage phase loss delay time, (sec)
R/W
Default:1
Range:1 to 3600
I_LINE_OC_ONSET
(ILineOCOnset)
49
Overcurrent onset threshold, (percent rated current)
R/W
Default:150 Range:100 to 200
I_LINE_OC_CLEAR
(ILineOCClear)
50
Overcurrent clear threshold, (percent rated current)
R/W
Default:140
Range:90 to 190
I_LINE_OC_DELAY
(ILineOCDelay)
51
Overcurrent delay time, (sec)
R/W
Default:5
Range:1 to 3600
I_LOAD_BALANCE_ONSET (ILoadBalanceOnset)
52
Load current balance onset threshold, (percent rated current )
R/W
Default:75
Range:10 to 90
I_LOAD_BALANCE_CLEAR (ILoadBalanceClear)
53
Load current balance clear threshold, (percent rated current )
R/W
Default:80
Range:10 to 90
I_LOAD_BALANCE_DELAY (ILoadBalanceDelay)
54
Load current balance delay time, (sec)
R/W
Default:4
Range:1 to 3600
I_LOAD_BALANCE_MIN_CURRENT (ILoadBalanceMin)
55
Load current balance minimum detect current, (percent rated current)
R/W
Default:50
Range:10 to 100
I_TUNE_OC_ONSET (ITuneOCOnset)
56
Tune overcurrent onset threshold,
(Percent rated current)
R/W
Default:150
Range:100 to 200
I_TUNE_OC_CLEAR (ITuneOCClear)
57
Tune overcurrent clear threshold,
(Percent rated current)
R/W
Default:140
Range:90 to 190
I_TUNE_OC_DELAY (ITuneOCDelay)
58
Tune overcurrent delay time, (sec)
R/W
Default:4
Range:1 to 3600
I_TUNE_UC_ONSET (ITuneUCOnset)
59
Tune circuit fundamental undercurrent onset threshold , (percent rated current )
R/W
Default:65
Range:10 to 100
I_TUNE_UC_CLEAR (ITuneUCClear)
60
Tune circuit fundamental undercurrent clear threshold, (percent rated current )
R/W
Default:70
Range:15 to 100
I_TUNE_UC_DELAY (ITuneUCDleay)
61
Tune circuit fundamental undercurrent delay time, (sec)
R/W
Default:3
Range:1 to 3600
I_TUNE_BALANCE_ONSET (ITuneBalanceOnset)
62
Tune circuit current balance onset threshold,
(percent rated current )
R/W
Default:75
Range:10 to 90
I_TUNE_BALANCE_CLEAR (ITuneBalanceClear)
63
Tune circuit current balance clear threshold ,
(percent rated current )
R/W
Default:80
Range:10 to 90
I_TUNE_BALANCE_DELAY (ITuneBalanceDelay)
64
Tune circuit current balance delay time , (sec)
R/W
Default:2
Range:1 to 3600
T_AMBIENT_OT_ONSET (TCtrlOTOnset)
65
Controls overtemperature onset threshold ,
(10 = 1.0 deg C)
R/W
Default:700
Range:100 to 850
T_AMBIENT_OT_CLEAR (TCtrlOTClear)
66
Controls overtemperature clear threshold ,
(10 = 1.0 deg C)
R/W
Default:600
Range:50 to 800
T_AMBIENT_OT_DELAY (TCtrlOTDelay)
67
Controls overtemperature delay time ,
(sec)
R/W
Default:5
Range:1 to 3600
STATUS_T_AMBIENT_UT_ONSET (TCtrlUTOnset)
68
Controls under temperature onset threshold,
(10 = 1.0 deg C)
R/W
Default:0
Range:0 to 0
EtherNet Only: Reserved Does not exist in Database
STATUS_T_AMBIENT_UT_CLEAR (TCtrlUTClear)
69
Controls under temperature clear threshold,
(10 = 1.0 deg C)
R/W
Default:0
Range:0 to 0
STATUS_T_AMBIENT_UT_DELAY (TCtrlUTDelay)
70
Controls under temperature delay time,
(10 = 1.0 deg C)
R/W
Default:0
Range:0 to 0
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal