Current Register Map

This register map contains parameters that are used to Line and Tune Currents in Amps RMS. Note that some parameters shown below may not exist in the parameter database/ or shown in PQVision. These parameters have been reserved for future use and are enabled in EtherNet/IP EDS File.
Note:
All parameters with an asterisk (*) in the description will require the Tech level access codes parameter key A: 0x007D (125) and parameter key B: 0xEA6E (60014). All parameters are enabled for communication to EtherNet/IP unless explicitly stated otherwise in the Notes Column of the Table.
Table
8
: Current Feedback and Setpoint Parameters Register Map
Parameter Name (EtherNet Name)
Instance ID
Description
Type
Default & Ranges
Notes
I_LINE_A_RMS (ILineARMS)
225
Line current phase A RMS, (10 = 1.0 Amps)
R
Default:0
Filter Input Current Phase A Range: 0 to 1000 Arms
I_LINE_B_RMS (ILineBRMS)
226
Line current phase B RMS, (10 = 1.0 Amps)
R
Default:0
Filter Input Current Phase B Range: 0 to 1000 Arms
I_LINE_C_RMS (ILIneCRMS)
227
Line current phase C RMS, (10 = 1.0 Amps)
R
Default:0
Filter Input Current Phase C Range: 0 to 1000 Arms
I_LOAD_A_RMS (ILoadARMS)
240
Load current phase A RMS, (10 = 1.0 Amps)
R
Default:0
Range: 0 to 1000 Arms
I_LOAD_B_RMS (ILoadBRMS)
241
Load current phase B RMS, (10 = 1.0 Amps)
R
Default:0
I_LOAD_C_RMS (ILoadCRMS)
242
Load current phase C RMS, (10 = 1.0 Amps)
R
Default:0
I_TUNE_A_RMS (ITuneARMS)
252
Tuned circuit current phase A RMS, (10 = 1.0 Amps)
R
Default:0
I_TUNE_B_RMS (ITuneBRMS)
253
Tuned circuit current phase A RMS, (10 = 1.0 Amps)
R
Default:0
I_TUNE_C_RMS (ITuneCRMS)
254
Tuned circuit current phase A RMS, (10 = 1.0 Amps)
R
Default:0
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal