Communication Register Map

This register map contains parameters which are used to communicate back and forth with the Harmonic Filter. Note that some parameters shown below may not exist in the parameter database/ or shown in PQVision. These parameters have been reserved for future use and are enabled in EtherNet/IP EDS File.
Note:
All parameters with an asterisk (*) in the description will require the Tech level access codes parameter key A: 0x007D (125) and parameter key B: 0xEA6E (60014). All parameters are enabled for communication to EtherNet/IP unless explicitly stated otherwise in the Notes Column of the Table.
Table
4
: Communication Feedback and Setpoint Parameters Register Map
Parameter Name (EtherNet Name)
Instance ID
Description
Type
Default & Ranges
Notes
BGM_MODULE_STATUS
(WLStatus)
293
Wireless pairing status
R
Default:0
Status of the BGM (Bluetooth LE module)
0 = Idle
1 = Advertising
2 = Connected
3 = Not Responding
4 = Radio Disabled
5 = Firmware Mismatch
SYS_INT_HB
(IntHeartbeat)
298
System interrupt heartbeat counter
R
Default:0
Range:0 to 65535
Processor Internal Heartbeat Counter Counts and rolls over to zero used to verify Processor Clock.
SYS_BG_HB
(BGHeartbeat)
299
System background heartbeat counter
R
Default:0
Range:0 to 65535
Processor background heartbeat Counter Counts and rolls over to zero used to verify processor clock operation
PARAM_KEY_A
(ParamKeyA)
4
Parameter access key value A
R/W
Default:0
Range:0 to 65535
Parameter Key Register A
User can write the required parameter access key to this parameter and Parameter Key Register B
To set the PQconnect board in a different access level.
PARAM_KEY_B
(ParamKeyB)
5
Parameter access key value B
R/W
Default:0
Range:0 to 65535
Parameter Key Register B
User can write the required parameter access key to this parameter and Parameter Key Register A
To set the PQconnect board in a different access level.
MB_SLAVE_ADDRESS
(ModbusDeviceID)
35
Modbus device server address
R/W
Default:10
Range:1 to 247
Modbus Slave Address
MB_BAUD_RATE
(ModbusBaud)
36
Modbus device baud rate,
(bits per second)
R/W
Default:11520
Range:0 to 11520
Modbus Baud Rate
11520 = 115200 baud rate
960 = 9600 baud rate
3840 = 38400 baud rate
MB_PARITY
(ModbusParity)
37
Modbus device parity
R/W
Default:2
Range:0 to 2
0 = None
1 = Odd
2 = Even
MB_SAVE_SET_FLAG
(ModbusSaveFlag)
38
Modbus RTU save new settings
R/W
Default:0
Range:0 to 2
Modbus Flag Save Settings
0 = Not Saving Settings
1 = Saving Settings"
BLUETOOTH_ENABLE
(BTEn)
158
Bluetooth radio enable
R/W
Default:1
Range:0 to 1
Set to Enable BGM
1 = Enabled
0 = Disabled
BGM_STATIC_PASSKEY_A
(WLPasskeyA)
174
Upper 16 bits of wireless password
R/W
Default:1
Range:0 to 15
BGM_STATIC_PASSKEY_B
(WLPasskeyB)
175
Lower 16 bits of wireless password
R/W
Default:45575
Range:0 to 65535
BGM_SECUIRTY_LEVEL
(WLSecurityLevel)
176
Wireless security level
R/W
Default:0
Range:0 to 1
BGM Security level.
High Security mode blocks new pairing requests. Passkey changes each time a connection is attempted.
0 = Low Security
1 = High Security
BGM_NUMERIC_ID
(WLNumericID)
177
Wireless numeric identifier
R/W
Default:0
Range:0 to 99
BGM_PAIRING_MODE
(WLPairingMode)
178
Wireless pairing mode request
R/W
Default:0
Range:0 to 1
0 = No active request
1 = Active request
BGM_COMMAND
(WLCmd)
179
Wireless command input
R/W
Default:0
Range:0 to 255
POWER_CYC_COUNT
(PwrCycCount)
188
Running number of powers on-off cycles
R/W
Default:0
Range:0 to 0
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal