Bluetooth Configuration

Bluetooth Configuration Summary
The Bluetooth section provides configuration options for the onboard Bluetooth device on every harmonic filter. Bluetooth will be enabled by default, and users can turn the Bluetooth module on or off at tech and factory access. Technicians can also modify the device identifier to a unique numerical value ranging from 0 to 99; however, this will require the user to save the settings afterward.
Device ID
The Bluetooth numeric identifier allows PQvision mobile to identify different filters within a 100ft range. The range for this Bluetooth Device ID is 0-99.
Security Options
The Filter’s Bluetooth device can be set to use basic or high security. Depending on the security level, the security settings will change to match the expected configuration.
  • Under basic security, the passkey used to connect via Bluetooth will match the Filter’s serial number. It can be changed via PQvision Desktop and the Add-On Profile, but it is not recommended unless warranted.
  • Under high-security access, the Filter has the option of accepting and denying any new connections, and a randomized passkey is created for every new connection. The current connection status of the Bluetooth module is also described and shown on the Bluetooth settings menu, which can be changed from connected to idle to not connected.
Connection Status Options
The Filter’s Connect status will determine if it is paired with another device. Possible Connection statuses are Idle, Advertising, Connected, Not Responding, Radio Disabled, and Firmware Mismatch.
Note
: The Connection Status Option, Not Responding, Radio Disabled, and/or Firmware Mismatch will only be detectable for PQconnect firmware version RevC3 and above.
Save Settings
Saves any modified settings so that they will remain after a power cycle. Saving the settings will automatically open the contactor.
Reset PQconnect
An easy and effective way to power cycle the Filter’s PQconnect board. Any unsaved settings will be lost.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal