Access Level Configuration
Configuration Access Summary
:This section focuses on setting the Access Level of the Filter. The Add On Profile contains several screens that allow the user to monitor and control the status of the Passive filter. Tech Access or Higher is required to view additional screens. Enter password
08252014
to enable tech access.Note:
If the Harmonic Passive Filter is connected via Bluetooth, the filter access configuration settings will return to the Basic/User access level. The mobile app access level will be the highest priority if connected, and the access level must be changed via the mobile app.Provide Feedback