Points view parameters
The
Points
view for the output devices includes these parameters:Parameter | Description |
Point | Displays the point number to which this configuration applies. |
Output State During Program Mode | Determines the behavior of each output when the controller transitions to Program mode. While in Program mode, outputs from the controller are ignored and the output behaves according to these:
|
Output State During Fault Mode | Determines what happens to the output of each point after a communication fault occurs and the device enters Communications Fault mode.
|
Fault Mode Output State Duration | Determines the length of time the Fault Value value is held prior to the Final Fault State. Tip : This parameter is not supported for the 5069-OW4I and -OX4I devices. |
Fault Mode Output State Final State | Determines whether the device transitions to On or Off after the Fault Mode Output State Duration elapses. The default final state is Off. If you choose Forever for Duration, you cannot choose a final state. The device retains its current Fault mode state. Tip: This parameter is not supported for the 5069-OW4I and -OX4I devices. |
Output State When Communications Fail in Program Mode | Determines the output action if communication fails in Program Mode.
|
Enable No Load Diagnostics | Determines whether No Load detection is enabled. No Load detects whether a signal wire has been disconnected from one of its terminals or the RTB has been removed. |
Diagnostics | Opens Ptxx Diagnostics for diagnostic information. |
See also
Provide Feedback