Ptxx Diagnostics parameters
Ptxx Diagnostics
includes these parameters:Parameter | Description | Value |
Short circuit fault | Shows whether an output short circuit or over-current fault is present on the point. |
|
Last fault timestamp for short circuit fault | Shows the timestamp of the last output short circuit or over-current fault in YYYY-MM-DD-HH:mm:SS_mmm (UTC-00:00) format.
| A valid time or None if there is no recorded event time. |
No load fault | Shows whether a no load fault is present on the channel. No load faults occur when a signal wire is disconnected from the output device terminal channel or the Removable Terminal Block (RTB) is removed from the device. |
|
Last fault timestamp for no load fault | Shows the timestamp of the last no load fault in YYYY-MM-DD-HH:mm:SS.mmm (UTC-00:00) format.
| A valid time or None if there is no recorded event time. |
Field power | Shows whether field power is present on the point. |
|
Field power on timestamp | Shows the timestamp of the last time field power turned on in YYYY-MM-DD-HH:mm:SS_mmm (UTC-00:00) format.
| A valid time or None if there is no recorded event time. |
Field power off timestamp | Shows the timestamp of the last time field power turned off in YYYY-MM-DD-HH:mm:SS_mmm (UTC-00:00) format.
| A valid time or None if there is no recorded event time. |
See also
Provide Feedback