Support

Website
Online support is available at the Spectrum Controls website (the "SC website") at www.spectrumcontrols.com. (use hotlink on AOP Vendor tab). See also "Documentation" section above.
Contacts
A list of distributors is available on the "SC website". Rockwell Automation currently provides telephone technical support for certain Spectrum Controls products. Contact numbers are as follows:
USA
1-440-646-6900
United Kingdom
01-908-635-230
Australia
1-800-809-929
Mexico
001-888-365-8677
Brazil
55-11-3618-8800
Europe
+49-211- 41553-630
or send an email to support@spectrumcontrols.com
For other locations, check the www.rockwellautomation.com/support website for Rockwell Automation Customer Support phone numbers. The support "Knowledgebase" at this website may contain information about known issues for this module. Prior to calling for technical assistance, please review Rockwell Automation information on testing your module.
Versions and Updates
The latest firmware version is 3.001 (as of August 2022). The hardware cannot be upgraded in the field.
Module Replacement
This module does
NOT
support RIUP (Removal and Insertion Under Power) from chassis while chassis power is applied. Reconfiguration of the module is not needed when replacing a module. Configuration data is retained in the controller and is sent to the module when the IO connection is established.
NOTE:
Proper handling precautions must be used to avoid damage to electronic components from Electrostatic Discharge. Refer to the "User’s Manual" for proper procedures.
Procedures and policies for returning a product to Spectrum Controls for service are available in the "User’s Manual" and on the "SC website". Your local distributor may also be able to provide information or assistance. Refer to the website for a list of distributors.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal