Function

The Compact 5000™ 5069-OV16F-SC and 5069-OV16FK-SC are 16-Point, 12/24 VDC fast digital sinking output modules designed to expand the local I/O capability of Rockwell Automation Compact 5000™ Systems. K versions of the module are conformally coated.
The module outputs digital signals provided by the PLC in sink mode.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal