Sample Projects

The RSLogix5000 ladder logic Sample Projects for the 1734sc-OE2CIH module demonstrate how to send HART messages to the module itself, acquire device specific data from the HART field device and other auxiliary functions.
NOTE
: The original Sample Projects for this module used the 1734 Generic Module profile. Please check the "SC website” for updated Sample Projects which use this custom Add-on-Profile.
Locating the Sample Projects
Some Sample Projects are installed with RSLogix5000. To locate them, select "Vendor Sample Projects" on the main RSLogix 5000 HELP menu. The latest version of the Sample Projects are also available from the "SC website”.
Using the Sample Projects
The Sample Projects can be used as a model for a separate application, as the start for a new project, or by copying or importing elements to another project. RSLogix5000 partial Import/Export can be used to add a sample project to an existing application project. This minimizes the number of user steps involved, and provides automatic checking and handling of conflicts with the existing project (e.g. duplicate tag names, etc.).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal