Sample Projects
The RSLogix5000 ladder logic Sample Projects for the 1734sc-IF4U module demonstrate how to interact with the module itself, acquire device specific data from the field device.
Locating the Sample Projects
Some Sample Projects are installed with RSLogix5000. To locate them, select "Vendor Sample Projects" on the main RSLogix 5000 HELP menu. The latest version of the Sample Projects are also available from the "SC website”.
Using the Sample Projects
The Sample Projects can be used as a model for a separate application, as the start for a new project, or by copying or importing elements to another project. RSLogix5000 partial Import/Export can be used to add a sample project to an existing application project. This minimizes the number of user steps involved, and provides automatic checking and handling of conflicts with the existing project (e.g. duplicate tag names, etc.). Refer to RA publication 1756-RM084K-EN-P, "Logix5000 Controllers Import/Export Reference Manual”, available for download at the Rockwell Automation website (www.rockwellautomation.com).
Provide Feedback