DeviceNet Scan List

TIP: Functions on this page are only available when the project is online.

Scanner Mode

Displays the scanner mode of the module.
Valid values are IDLE and RUN.

Enable AutoScan

Enables or disables the AutoScan feature.
When set to enable (and the previous value was disable), the existing scan list shall be cleared.
Any set access to the Scan List from a tool such as RSNetworx shall disable AutoScan.
This value can be set only when the scanner is in IDLE mode and is saved to non-volatile memory immediately.

Bytes per Node

Choose the size of the input and output memory maps that the scanner will allocate for each device it detects on the network during AutoScan.
Valid values range from 1 to 32 bytes per node.

Devices in Scan List

Indicates which device addresses the scanner has in its internal scan list.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal