DeviceNet Configuration
DeviceNet File
Displays the name of the DeviceNet file you want to associate with the module. By
default, this field is blank.
TIP:
The file name will be saved with the Logix
Designer project. However the .dnt file itself, or its contents, is not stored with
the project.
Launch RSNetworx
Click this button to launch RSNetWorx for DeviceNet, from which you can view and edit
the DeviceNet network. Network data is stored in the selected DeviceNet file
(*.dnt).
Provide Feedback