Troubleshooting
IMPORTANT:
Before attempting to maintain or troubleshoot a
system, read the detailed module information and IMPORTANT safety recommendations in the
ILX56-PND User Manual. Refer to the Diagnostics chapter for information.
Status/Diagnostics
In addition to the LCD and LED displays on the module, RSLogix5000 and Studio 5000 Logix
Designer software indicates module fault conditions in the following ways:
- Warning signal on the main screen next to the module when the IO connection is broken
- Status on the Device Information Page
Refer to the ILX56-PND User Manual for detailed information on status, diagnostics, error
codes, and alarms.
Module Reset
The module can be reset using the Reset Device option within the Module Info page.
Calibration
This module does not require calibration.
Provide Feedback