General
This "Basic Module Information" (BMI) provides quick access to a list of the main
module functions, some attributes, and the location of more detailed module information.
IMPORTANT:
When developing an application, or
troubleshooting a significant problem, it is IMPORTANT to read and follow more detailed
module information, including safety recommendations. The primary source of detailed module
information is the ILX56-PND User Manual, which is available for download from the ProSoft
Technology, Inc. website (www.prosoft-technology.com).
Function
The ILX56-PND PROFINET Device module allows Rockwell Automation® ControlLogix® processors
to communicate on a PROFINET RT protocol network as a PROFINET device.
This module supports up to 4096 bytes of input and output data as high-speed cyclic I/O
data on a PROFINET RT network.
Combined with the use of multiple I/O connections with the ControlLogix processor, this
module provides data update rates that will meet even the most demanding of PROFINET RT
applications.
Configuration
The easy-to-use configuration utility, ProSoft PLX50 Configuration Utility, is used to
configure the PROFINET network.
Module Identity
Vendor ID: 309 Vendor Name: “ProSoft Technology”
Product Type: 12 Product Type Name: “Communication”
Product Code: 5116 Catalog Name: “ILX56-PND”
Communication
Specification | Description |
|---|---|
Total Cyclic Data | Maximum 4096 Input Bytes and 4096 Output Bytes |
Acyclic Data | Parameter Data via Read/Write Record |
Redundancy | Higher availability through Media Redundancy Protocol (MRP) Ring
Redundancy |
Conformance Class | Class B |
Provide Feedback