Documentation

Downloads

The primary source for detailed information about this module is the ILX56-PNC User Manual. Available for download from the ProSoft Technology, Inc. web site at www.prosoft-technology.com are:
  • User Manual and Datasheet
  • Presentations, Application stories and setup videos may also be available
  • Add-On Profile, EDS file, PLX50 Configuration Utility.

EDS File

The EDS file is used for identifying the module to network tools, such as RSNetWorx or a CIP (refer to “CIP” in RSLogix5000 HELP) network browser (e.g., RSLinx Who). The EDS file can be downloaded from the ProSoft Technology website at www.prosoft-technology.com, and installed using the RSLinx Hardware Installation Tool.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal