Configuration
Add-on Profile (AOP)
The module's backplane functionality is configured through a custom, separately-installable
Add-on-Profile within RSLogix5000 or Studio 5000 Logix Designer Software. When a module from
the RSLogix5000 or Studio 5000 Logix Designer Select Module dialog is added to the project
tree, the following items are created in the project:
- Producer/consumer IO connections using the module's specific IO assemblies and sizes.
- Module Info tab which displays the Module Identification information and Module Status information.
- PROFINET Configuration tab which allows AOP to launch the configuration utility to configure PROFINET Network.
- Vendor tab which displays the basic information about ProSoft Technology.
Module Configuration Pages
There are no custom configuration pages for the module.
Provide Feedback