Connection View
Use the Connection view to specify controller-to-device connection configuration.
- Select a requested packet interval.
- Choose to inhibit the device connection(s).
- Configure the controller so that a loss of connection to this device causes a major fault in the controller.
- View connection faults.
TIP:
The single connection configuration displayed on the
Connection view sets the parameters for ALL connections between the controller and
device.
Provide Feedback