Troubleshooting
NOTE:
NOTE: Before attempting to maintain or troubleshoot a system, read the detailed module information and IMPORTANT safety recommendations in the Remote Access A/C Manual and the Remote Access Control Manual. Module Indicators/LEDs
Refer to the section on "Indicators and LEDs".
Module Reset
The module can be RESET from the button in the AOP. Refer to the Remote Access A/C Manual and the Remote Access Control Manual for other Reset methods.
RSLogix5000 Diagnostics
RSLogix5000 software indicates module fault conditions in the following three ways:
- Warning signal on the main screen next to the module, when the IO connection is broken.
- Fault message in a screen’s status line, with notification in the Tag Editor. General module faults are also reported in the Tag Editor. Diagnostic faults are only reported in the Tag Editor.
- Status on the Module Info Page.
Refer to the Remote Access A/C Manual and the Remote Access Control Manual for detailed information on status, diagnostics, error codes, and alarms.
Provide Feedback