Indicators and LEDs
The Ethernet/IP communication module is equipped with LEDs which signal the module and
communication state.
LED locations

LED State | Description |
|---|---|
Off | No power or no IP address |
Green | Online, one or more connections established (CIP class 1 or 3) |
Flashing Green | Online, no connections established |
Red | Duplicate IP address, FATAL error |
Flashing Red | One or more connections timed out (CIP class 1 or 3) |
LED State | Description |
|---|---|
Off | No power |
Green | Controlled by a Scanner in Run state |
Flashing Green | No configured, or Scanner in Idle state |
Red | Major fault (EXCEPTION state, FATAL error, etc.) |
Flashing Red | Recoverable fault(s) |
Provide Feedback