Documentation

Manual

The primary sources of detailed module information is the Memograph M RSG45 EtherNet/IP manual. It can be found on the CD or on the Endress+Hauser website (www.endress.com/RSG45).

EDS File

The EDS file is used for identifying the module to network tools, such as RSLinx, RSNetWorx or a CIP (refer to "CIP" in RSLogix5000 HELP) network browser (e.g. RSLinx Who). It can also be downloaded from the Endress+Hauser website. The ESD file is installed using the RSLinx Hardware Installation Tool.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal