Documentation
Manual
The primary source for detailed information about this module is the Endress+Hauser
document, “Promass 100 EtherNet/IP Supplementary Documentation”, available for download from
the Endress+Hauser website (www.endress.com).
EDS File
The EDS file is used for identifying the module in network tools, such as RSNetWorx or in
CIP (refer to “CIP” in RSLogix 5000 HELP) network browser (e.g. RSLinx Who). The EDS file
can be downloaded from the “Endress+Hauser website” and installed using the RSLinx Hardware
Installation Tool.
Certifications
Certifications for this module normally include CE. Refer to the markings on the
transmitter nameplate and to the specifications in the Promass 100 Operating Instructions
for more detailed information. Products with a CE mark are approved for installation within
the European Union and EEA regions.
Provide Feedback