Documentation
Manuals
The primary source for detailed information about this module is the Endress+Hauser
document, “Promag 400 EtherNet/IP Supplementary Documentation”, available for download from
the “Endress+Hauser website”.
EDS File
The EDS file is used for identifying the module in network tools, such as RSNetWorx or in
CIP (refer to “CIP” in Studio 5000 Logix Designer HELP) network browser (e.g. RSLinx Classic
RSWho or FactoryTalk Linx Network Browser). The EDS file can be downloaded from the
“Endress+Hauser website” and installed using the EDS Hardware Installation Tool. The EDS
file is also embedded in the Promag 400 and can be extracted by RSLinx Classic or
FactoryTalk Linx.
Certifications
Certifications for this module normally include CE. Refer to the markings on the
transmitter nameplate and to the specifications in the Promag 400 Operating Instructions for
more detailed information. Products with a CE mark are approved for installation within the
European Union and EEA regions.
Provide Feedback