General
Designated Use
Electromagnetic flow measurement has been in use around the world for over 50 years, as
witnessed by the popularity of these meters that continues unabated in virtually all sectors
of industry. Electromagnetic flowmeters can be used to measure all electrically conductive
liquids (> 5 µS/cm) with or without solids, e.g. water, wastewater, sludge, slurries,
pastes, acids, alkalis, juices, fruit pulp, etc. In the industrial environment, sectors that
utilize this measuring principle include: water/wastewater, chemicals, pharmaceuticals, pulp
and paper, foodstuffs, etc. Electromagnetic flowmeters are even robust enough to be used in
mining. Resulting from incorrect use or from use other than that designated the operational
safety of the measuring devices can be suspended. The manufacturer accepts no liability for
damages being produced from this.
Connection versions
The measuring device can be connected to the EtherNet/IP network in one of three ways.
Refer to the “Supplementary Documentation” for information on how to connect the device to
an EtherNet/IP network.
Measuring device
The measuring device has an Ethernet module to connect it to an EtherNet/IP network and for
connecting to the integrated Webserver. It uses the EtherNet/IP communication protocol
(Ethernet Industrial Protocol) in accordance with the ODVA specification.
Data
The main measuring values are transmitted via EtherNet/IP communication. The sequence of
the input and output values can be configured via the local display as well as via the
integrated Webserver. Refer to the “Supplementary Documentation” for further
information.
Communication
EtherNet/IP Network
- Ethernet switch settings
- 10 or 100Mbps
The default IP and MAC addresses are printed on the connections nameplate
Provide Feedback