Configuration

Add-on-Profile (AOP)

The module functionality is configured through a custom, separately-installable Add-on-Profile within RSLogix 5000 Software. When a module from the RSLogix 5000 Select Module dialog is added to the project tree, the following items are created in the project:
  • a custom Module-Defined Data Type, and corresponding Input, Output Tags
  • a producer/consumer IO connection using the module’s specific IO assemblies and sizes.

DIP Switches for hardware addressing

The IP address of the measuring device can be configured for the EtherNet/IP network using the DIP switches. Addresses in the range from 0 to 254 are permitted (the address 255 is reserved for the broadcast address).
The IP address for software addressing is active when the device leaves the factory (default IP address: 192.168.1.212), i.e. all the DIP switches for hardware addressing are set to OFF.
Switches 1-8 configure the last three digits (last octet) of the IP address. The first three octets can be configured via software addressing to reflect the desired hardware IP address.
Setting the EtherNet/IP address with switches
dipSwitches
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal