Analyzer Information
General - HwVersion Actuator
(class 0x313, instance 1, attribute 12)
Hardware version of the device.
General - Software version
(class 0x313, instance 1, attribute 13)
Software version of the device.
General - Mode
(class 0x313, instance 1, attribute 14)
Operation mode.
Value | Operation Mode |
|---|---|
0 | Manual |
1 | Automatic |
2 | Fieldbus |
General - Activity
(class 0x313, instance 1, attribute 15)
Current activity.
Value | Activity |
|---|---|
1 | Measurement |
2 | Calibration |
3 | Cleaning |
4 | reserved |
5 | reserved |
6 | Emptying |
7 | reserved |
8 | reserved |
9 | Rinse hoses |
10 | Initializing |
11 | Cleaning up |
12 | Cleaning sample preparation |
13 | Dispenser replacement to top |
14 | Dispenser replacement to bottom |
15 | Testing liquidmanager actuator |
16 | Bottle insertion |
17 | Bottle removal |
18 | Open valves |
19 | Close valves |
20 | Rinse reagents |
21 | Rinse analyzer |
General - Remaining time
(class 0x313, instance 1, attribute 16)
Remaining time of current activity.
General - Power fail reaction
(class 0x313, instance 1, attribute 3)
Powerfail reaction.
General - Sample Preparation Installation
(class 0x313, instance 1, attribute 52)
Availability of sample preparation.
Operation time - Filter mat
(class 0x313, instance 1, attribute 17)
Operating time of filter mat.
Photometer - Hardware version
(class 0x313, instance 1, attribute 35)
Hardware version of photometer.
Photometer - Software version
(class 0x313, instance 1, attribute 36)
Software version of photometer.
Photometer - Operation time
(class 0x313, instance 1, attribute 37)
Operating hours of photometer.
Photometer - Temperature
(class 0x313, instance 1, attribute 38)
Temperature of photometer cuvette.
Photometer - Raw measurement value
(class 0x313, instance 1, attribute 39)
Raw value of photometer.
Provide Feedback