Volume & Mass Totalizers
Counting Direction
By default, the counting direction of all totalizers is Positive Only.
The possible counting directions are:
Counting direction | Totalizer function |
|---|---|
Positive Only | The totalizer counts the quantity of liquid that flows in the direction defined
as positive, i.e. in the same direction as the arrow located on the front of the
device. |
Negative Only | The totalizer counts the quantity of liquid that flows in the direction defined
as negative, i.e. in the direction opposite to the direction of the arrow located on
the front of the device. |
Positive and Negative | The totalizer counts the quantity of liquid that flows in the direction defined
as positive but deducts the quantity of liquid that flows in the direction defined
as negative |
Provide Feedback