Temperature
Damping
The damping makes it possible to damp the fluctuations of the measured values of the
temperature:
- on the FLOWave display,
- on the PLC inputs.
The damping is not applied to the new measured value if the 2 following conditions are met:
- a Low, Medium or High damping level is active,
- and the variation between 2 values that are measured one after the other is higher than 20 °C.
By default, the measured temperature values are not damped.
Damping level | Response time |
|---|---|
None | 0 s |
Low | 1 s |
Medium | 10 s |
High | 30 s |
Provide Feedback