Event Configuration
6 Sensor events can trigger the global NAMUR NE107 status (None, Failure, Out of Spec,
Maintenance) of the transmitter device.
Special event in the process | Meaning | Special condition |
|---|---|---|
Not totally filled | The tube is not totally filled. | Not all the sensors are in contact with the liquid. |
Liquid out of range | The speed of sound in the liquid is out of range. |
|
Unstable flow | The flow rate is not stable. | The standard deviation of the flow rate measurements is too high. |
Low flow cut off | The cut-off value of the flow rate has been used. | The cut-off function must be enabled |
Change of liquid | A different liquid flows in the pipe. The message is active for 10 s on the
display. | The speed of sound in the liquid has changed by more than 3 m/s in
1 second. |
Backward flow | The liquid flows in the opposite direction as the one set as positive direction
of the flow. |
Provide Feedback