Acoustic Transmission Factor
The acoustic transmission factor makes it possible to know the quality of the transmission of
sound in the liquid thus the reliability of the measurements.
Indeed, the wave transit time in the liquid and the wave amplitude change depending on the
following criteria:
- the type of liquid: aqueous solution, oil solution, emulsion, …
- the presence of gas bubbles,
- the presence of solid particles,
- the liquid temperature,
- the DN of the pipe.
The temperature changes of the liquid are not compensated for the measurement of the acoustic
transmission factor.
The device measures acoustic transmission factors from 10 % and up.
If the wave amplitude in a liquid flowing through the pipe is higher than the wave amplitude
in water, the measured acoustic transmission factor will be higher than 100 %.
If the wave amplitude in a liquid flowing through the pipe is lower than the wave amplitude
in water, the measured acoustic transmission factor will be lower than 100 %.
Gas bubbles or solid particles in the liquid have a similar effect on the transmission
acoustic factor. If the concentration of gas bubbles or solid particles increases in a liquid,
the acoustic transmission factor decreases. So, measuring and monitoring the acoustic
transmission factor can be used to detect the presence of gas bubbles or solid particles in
the liquid.
Take into account that special process conditions can have an effect on aging of the sensor
thus on the acoustic transmission factor value.
Damping
The damping makes it possible to damp the fluctuations of the measured values of the
acoustic transmission factor:
- on the display,
- on the totalizers,
- on the outputs.
The damping is not applied to the new measured value if the 2 following conditions are met:
- a Low, Medium or High damping level is active,
- and the variation between 2 values that are measured one after the other is higher than 30 %
The Low damping level or no damping at all (None) are suited for applications/processes
that need fast response times.
The Medium damping level or the High damping level are suited if the values of the acoustic
transmission factor change slowly.
Damping level | Response time |
|---|---|
None | 0 s |
Low | 1 s |
Medium | 10 s |
High | 30 s |
Provide Feedback