DANGER: Device configured for Unicast connections

Device is configured for Unicast connections. Unicast connections cause Disqualification (DISQ) and do not allow Qualification (SYNC).
The controller is enabled for redundancy and a unicast connection is configured. For the redundant controller to stay synchronized, set connections to multicast.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal