DANGER: Connection Loss
Clearing
Enable Supervisor Mode
indicates that this device is no
longer a Device Level Ring supervisor. This may disrupt (break) the connections to every
device on the ring if this device is the only supervisor on the ring.Before proceeding ensure that loss of all connections traversing the ring at this time is
acceptable.
If a connection disruption is acceptable at this time:
- In the confirmation dialog box, selectYes.
- Otherwise, selectNoto cancel the operation.
Provide Feedback